Hi Team,
Customer want to know if there is a way to use SAR ADC (such as ADS8900B) to create a "sound card" that can be recognized as such by an OS. Below is the details.
"After a rather long series of reflections on an ADC that might "really work" as an audio measurement tool for THD and S / N on a BW of a few hundred kHz, I am afraid that the commercial sound card option, and in general, the use of delta-sigma ADC is limiting in terms of BW (and in some cases also THD, S / N and distortion) while the SAR option, which could extend BW up to almost 500kHz and have a very small form factor, thanks to the possible use of Raspberry pi to manage the measurement software, it requires heavy development both hardware and (even more) software as applications such as REW, and most likely also Digilent Waveforms, require the OS to recognize the device as a sound card. Is there a way to use a SAR ADC (such as ADS8900B) to create a "sound card" that can be recognized as such by an OS?"
Thank you in advance.
Regards,
Maynard