I have question concerning notes 8 and 9 in the AMC7812 datasheet. Do these notes supersede the table entries? I intend to supply the device with AVDD = AVCC = DVDD = 5 V and IOVDD = 3.3 V. Can I pull up the GPIOs to 5 V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have question concerning notes 8 and 9 in the AMC7812 datasheet. Do these notes supersede the table entries? I intend to supply the device with AVDD = AVCC = DVDD = 5 V and IOVDD = 3.3 V. Can I pull up the GPIOs to 5 V?
Hi Paul
Thanks for the reply. My question is related to the table above. When IOVDD = 3.3 V, then - according to the table - the maximum GPIO voltage is 0.3 V + 3.3 V = 3.6 V. However, the notes imply that the pull-up voltage can be higher.
Can you confirm that the pull-up voltage at the GPIO pins can be 5 V although IOVDD is only 3.3 V.
Kind regards
Frank
Only GPIO0-3 can be pulled up to 5V. GPIO4-7 is limited to 3.3V. So you cannot configure all of the GPIO pins to the use the same pullup unless you are connecting them to IOVDD.
Thanks,
Paul