This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DAC5682Z: DAC5682Z evm GUI

Prodigy 70 points

Replies: 3

Views: 213

Part Number: DAC5682Z

Hi 
Does anybody know can we use Ti evm gui's with our designs or not? I mean the gui is board specified or not? 

  • anybody?
  • Hi John,

    The EVM GUI is intended to be used with the EVM and the general purpose evaluation. The EVM does have the ability to dump out working set of register writes to allow you to implement the working register writes into your design. You will have to implement these register writes with your own SPI bus tool and communication protocol. If you are thinking about using the same FTDI USB chip in your design you also consider using the Labview based DLL. You may visit the following forum thread with people discussing integrating the DLL into their program. One person was able to integrate it with the DAC5682z EVM.

    https://e2e.ti.com/support/data-converters/f/73/p/432855/1629194?tisearch=e2e-sitesearch&keymatch=dac348x%20ftdi#1629194

    -Kang

  • In reply to Kang Hsia:

    Hi Kang!
    Thank you for your great help.
    As always Ti is the best.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.