This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TSW14J57EVM: TSW14J56 backwards compatibility

Prodigy 20 points

Replies: 2

Views: 59

Part Number: TSW14J57EVM

I am interested in evaluating the ADC08DJ3200 and I already have the data acquisition board TSW14J56. Can I use this board with the ADC08DF3200EVM or do I have to purchase the newer TSW14J57?

  • Hi
    The ADC08DJ3200EVM can be used with the TSW14J56EVM Rev. D and later boards. This configuration will be limited to the ADC08DJ3200 device JMODE and clock frequency settings with 8 or fewer serial lanes, and with serial data rates up to 10 Gbps.
    This will enable usage in dual or single input modes up to the maximum clock frequency (3200 MHz) using JMODEs 5 and 7. (See ADC08DJ3200 datasheet Table 10).
    I hope this is helpful.
    Best regards,
    Jim B
  • In reply to Jim Brinkhurst84999:

    Thanks for the quick response Jim B

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.