Rafael -
I started having been having problems with the AMC6821EVM-PDK kit today. I think I offset the fan connector when I was plugging it into J1. I'm not sure which way I went. It seems the fan isn't getting the PWM signal, even though it shows up & changes in the registers. Also, the fan TACH isn't showing up or changing in the registers. It seems like something on the board is damaged. Any thoughts on where to look?
Also, note that on power up, the AMC6821EVM has two red alarm leds set: THERM and FAN. Also, the LOCAL temp is pegged at 99C, but the remote temp is responding correctly.