This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1200EVM vhdl

Other Parts Discussed in Thread: ADS6149, ADS5463, ADS5281

I am evaluating this board with ADS4146EVM and noticed there is no enough files. Please, send me vhdl code and ucf file for TSW1200EVM at hdmb63@gmail.com. 

 

  • Hi,

    Sent to the address provided.  We did not write the TSW1200 code in VHDL, but rather Verilog.  Also, i don't know what you mean by not enough files, as the source code is not normally provided with the hardware and User Interface but rather upon request.

    Regards,

    Richard P.

  • Dear sir.

    Can I receive verilog code & FPGA binary ?

    plz help me.

    popradtatri@gmail.com

  • Hi,

    You've appended your request for the source code in two places, one was in reference to serialized data formats and this one which is in reference to parallel DDR data formats. I need to know whether you want the TSW1200 code for parallel DDR LVDS data formats or serialized LVDS data formats. 

    Regards,

    Richard P.

  • Hi,

    Can I get a Verilog top module with complete pin list and UCF file (for ISE) with pin assy and global constraints - all non related to a specific design.

    Thanks,
    Eli.
  • Eli,

    when you say non-related to a specific design, I am guessing that our source code for the LVDS parallel bus format would be best suited.  The source code defines inputs to the FPGA for all the possible LVDS pairs that are listed in the schematics for the TSW1200 connector regardless of whether a specific EVM uses those inputs or leaves them floating.   Also the zip file includes the ucf file.    There are a few examples of timing constraint in the UCF for the DDR inputs, with one example for a source synchronous timing such as from our ADS5463 EVM and the other for a source centered timing such as our ADS6149.  But I believe Xilinx has changed the syntax since then for handing the DDR timing constraints.

    The other design database I could have sent would have been for our pseudo-serialized format such as our ADS5281, and the constraint file for that lists only as many as 10 LVDS inputs for just those inputs that are used by our highest channel count device.

    Anyway, if you would provide an email address to send it to I can send that out.

    Regards,

    Richard P.

  • Hi Richard,
    Thank you for the prompt reply.

    You got a point there with the LVDS pins, I don't know yet if serial or parallel I/F will be used so best to have both examples.
    As for pin assignment and constraints I was not referring specifically to LVDS pins but a complete pinout (clocks, headers, leds, switches , lvds_pairs, etc ...)

    My email is: egoldman@airspan.com

    Appreciate your support.

    Thanks,

    Eli.

  • Sent to the address provided.

    Regards,

    Richard P.