Other Parts Discussed in Thread: ADS1298
Hello,
If I send the START OPCODE to the ADS1298 followed
by the RDATAC OPCODE, the DRDY pin toggles as expected. If I send the STOP
OPCODE to the ADS1298 the DRDY pin stops toggling. So all looks
fine. Now I want to read the converted data. I start conversion and now I can
read one or two data packages. After this, the DRDY stays high and there is no
possibility to leave this state. No reaction to the reset pin or the power down
pin. I cannot restart the conversion. But in this state I can read/write the registers
correct… Only a complete power reset (power switch off-on) can leave this
state.
If I use the start pin the communication works fine?
Is this a known problem?
mfg
uwe