This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC7528 Dual DAC Outputs not operating the same

Other Parts Discussed in Thread: TLC7528, OPA627

I am using both DACs in a TLC7528 and I am not seeing the same output characteristics on both DACs.  I am updating DACA and DACB 250 nanoseconds apart at a 1Khz rate.  My test case is setting both DACs from all 0's to full scale.  VDD=+5V and both reference voltages are -6V.

DACA transitions to full scale in ~1usec but DACB takes much longer ~200usec to eventually transition to full scale.

I believe I am meeting all of the setup and hold time requirements of the device per the data sheet but I could not find any specification about time between DACA and DACB updates.

Has anyone used the TLC7528 or similar device that could help?