Hello,
I have an ADS1298 kit and I developed a board of my own using an MSP430f5529 to communicate with the ads1298 board. Everything worked just fine.
Recently I bought an ADS1198 kit and when I tried to use it with the same MSP430 board, it didn't work. The ADS1198 board is working with the MMB0 board, but not with mine.
When I watched the SPI SOMI with the oscilloscope, I noticed that the board is triggering DRDY, but when the SCLK is sent, nothing comes out of the SPI.
The registers values are set the same way that the LabView software does, the AVDD and DVDD are configured the same way my ADS1298 was and the initialization sequence is also the same I used on my ADS1298.
Any idea what could be wrong?
Thanks,
Gean Chu