This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with ADS62P29 Eval Board USB Driver for SPI Interface

Other Parts Discussed in Thread: ADS62P29, ADS62P49

Hello everyone,

I am trying to use the ADS62P29 Eval Board with an Altera Cyclone 3 FPGA Development Kit. 

I want to use the TI SPI Software to set up the ADC to test-mode to verify the connection to the FPGA Board. I installed the SPI Software including the USB drivers. 

I am using the USB Blaster to programm my FPGA. 

When i plug in the USB cable to connect the ADC Board to my computer the hardware is not recognized. But if use the Altera Programmer software to "scan chain" the TI SPI interface shows up in my hardware manager for a few seconds and then disappears again. I am using Windows 7 32 Bit OS. I also tried to connect the ADC Board via USB to a Windows XP computer, but this one doesnt recognize it either!

When I try to write ADC registers via the SPI software, the following error message occurs : Error 1 occured at FT_SetBitMode: Set Bit Bang

Does anyone have a solution for this problem?

Thank you so much in advance!