I am having issue with a 4-20 ma measurement loop. The circuit is designed as follows, with the output connected to a 16-bit ATD (ADS8344). Not my selection, it is standard on the micronontroller board.
I am attempting to inject a signal with a 4-20 ma calibrator to verify operation, but am getting the following output:
| PART_CNT1 | Current (mA) | ATD Counts1 | Vin @24.9ohm | Scope Volts* | Scope Volts** | ATD Counts2 |
| 0 | 236 | 0 | 0.121 | 0.157 | 256 | |
| 2 | 8095 | 0.0498 | 0.675 | 0.684 | 8000 | |
| 4 | 12799 | 0.0996 | 1.11 | 1.13 | 13167 | |
| 6 | 16703 | 0.1494 | 1.63 | 1.67 | 18751 | |
| 8 | 19807 | 0.1992 | 2.1 | 2.1 | 24047 | |
| 10 | 23135 | 0.249 | 2.57 | 2.61 | 27551 | |
| 12 | 26496 | 0.2988 | 3.1 | 3.1 | 32127 | |
| 14 | 29951 | 0.3486 | 3.52 | 3.55 | 37055 | |
| 16 | 33631 | 0.3984 | 4.06 | 4.08 | 41855 | |
| 18 | 37759 | 0.4482 | 4.5 | 4.51 | 46591 | |
| 20 | 65407 | 0.498 | 4.97 | 5 | 65279 |
Where: Current - the value injected at the amplifier inpu to produce the output response
Vin @24.9ohm - input voltage measured across the 24.9 ohm resistor
ATDCounts1 - The ADC reading with no scope attached to the AD627 output
ScopeVolts* - Voltage measured at AD627 output with ADC OFF.
ScopeVolts** - Voltage measured at AD627 output with ADC ON and acquiring data.
ATDCounts2 - ADC reading taken in conjunction with ScopeVolts**.
(SEE PLOTS BELOW)
OK, this is what I did, I connected the current source input of the AD627 AMP test and connected a scope probe to the output of the AD627.
1)Test circuit with no scope attached to amp output. Read ADC value from microcontroller. (See ATDCounts1)
2) Repeated test with scope attached to output of AD627. I ran the test first with the ADC OFF (see Scope Volts*) Then I repeated the test with the ADC ON (See Scope Volts** and ATDCounts2).
I plotted these valuse as shown above.
So, the question is, since the amplifier response seems very linear over the entire range of values for both cases, scope attached and not attached.
What is causing the large noticable change in slope in the ADC response?
The design is such that the amplifier is driving the ADC input directly. So, DC coupled, and also no matching or compensation networks.
Any suggestions?
Thanks