Technical Ref Doc states (p.12) that if the RLDIN/RLDREF pin is not used it should be connected to AVdd. This appears to be incorrect. My investigation indicate that if irit is taken to AVdd then RLDout is always near AVdd, irrespective of the setting if RLDREF (internal or external). It appears that RLDIN/RLDREF needs to be kept at near (AVdd-AVss)/2 - but then is left to wonder whether the RELREF int/ext switch actually works or not.
In the case of the ADS1292 Dev Boards, RELDIN/RLDREF is held at near the RLDout portential courtesy of a 100K resistor, obstensively there to allow the RLD signal to be fed to RLDIN for measurement, but it seems this is not optional.
RLDIN/RLDREF can be used as an auxiliary input to the MUX (a 4th input) and I had hoped to use it as such (and not for measuring RLD) however it seems one needs to be careful about how one does the biassing.
Appreciate id anyone out there has also come to the same conclusion.
tks, bruce
(love the chip)