This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

code example to ADS7863

Prodigy 55 points

Replies: 8

Views: 1476

Hi to everyone.

Someone can to help me. I looking for code example to use ADC (ADS7863). It use SPI interface.

  • Hi Yuri,

    Welcome to our forum!  Is there any particular processor you have in mind to use with the ADS7863?

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    i want to use raspberry pi (ARM)  with ADS7863EVM (board). i need some example (in C) to learn to config SPI registers to convert and sampling with it adc. 

  • In reply to yuri yuri:

    Hi Yuri,

    I have no SPI examples for the Raspberry Pi, however, there are several code snippets available for the ADS8361 and ADS7861 on various TI processors here: http://www.ti.com/product/ads8361#doctype1

    The ADS8361 and ADS7861 are early version of the ADS7863, they did not have the internal reference, so there are no actual 'registers' to configure.

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    Tom Hendrick
    however, there are several code snippets available for the ADS8361 and ADS7861 on various TI processors here: http://www.ti.com/product/ads8361#doctype1

    i can't to find the examples.

  • In reply to yuri yuri:

    Yuri,

    Did you have any luck finding some example code? I also want to interface to a ADS7863 although I am using a TI MSP430F5528. I have used the built in SPI port before and I'm sure I can figure it out but some example code would be a big help. 

    Mike

  • In reply to yuri yuri:

    Hi Yuri,

    How are you making out here?  I'll see what I can do about getting you some example code after the first of the new year.

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    Thanks Tom 

    If you can to take me an example i'll be very grateful. 

  • In reply to Tom Hendrick:

    I would like to see some example code for this particular application as well. Any help would be greatly appreciated!
    Thanks!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.