I am using THS4509 to drive ADS4242. I have following doubts about this combination.
on the page 80 of the datasheet it is mentioned that termination resistors are connected to 1.5V VCM of the device
Why these values of VCM is different? Which is correct value?
If I am using THS4509 cant I connect ADC VCM directly to THS4509? I am operating THS4509 at -Vss=0V to +Vss=5V, Would there be any issue if I connect common mode of THS4509 to 0.9V VCM of ADC as this VCM is less then mid supply voltage of THS4509?
- Which scheme is better, connecting VCM of ADC to THS4509 common mode or connecting VCM of ADC through 24.9 ohm resistor and keeping commond mode of THS4509 at 2.5V mid supply range?