Hello,
Currently I'm in a project where I'm building a prototype to oversample a signal around 5 MHz and perform signal analysis on a DSP. My previous equipment was a TMS320F28335 experimenters kit with an internal 12-bit 12.5 MSPS ADC. Now I would need a memory upgrade and a better external ADC (no DSP with internal ADCs exists with more RAM and sample rate). I've made a post in the microcontrollers forum (http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/246037.aspx?pi239031349=1), but thought that this forum would have better ideas regarding the ADC and how to connect it.
Because I think that 12-14-bit 65 MSPS would be enough and will not give me too much data to handle, I've looked into ADC specs similar to that. But you should know that I have no experience in this field other than that I gained by using the F28335. Because I'm more on a time budget than a price budget, I'm thinking of evaluation modules to get rid of hardware troubles. One example is the ADS62P42 evaluation module. How could this be connected to a DSP (e.g. C2000/C6000 family experimenters kit)? From what I've understood, a 65 MSPS sample cannot be pipelined directly to a DSP because of lack of CPU speed? With this in mind, I found the low cost capture card TSW1405EVM. This can save 64 kB of the sampled signal, which in my case would be enough (I expect only ~6000 samples).
Is a possible combination a ADS62P42 to sample the signal, a TSW1405EVM to connect to the ADC and save the sampled signal, and then a DSP (e.g. C28346 experimenter's kit or similar) to retrieve this signal in order to perform signal processing? How much work would it require to put this all together? My thought was that because they are all evaluation modules and experimenter's kits, it would simply be some wiring and programming. In the end, I want the DSP to be the master, i.e. to initiate when the ADC should start sampling and for how long (with an ADC internal clock). This must be driven by the DSP code without PC software GUI.
Any other ideas of what I can do is also much appreciated.
Best regards,
Fredrik