We have an application using the SN65LBC176A-EP for RS485 communication with 2 nodes. We are seeing failures on a node when the RS485 Master is dropped/removed from the line. The failure presents itself as power ground short on the PCB with the node. Removing one of the nodes does not damage the Master however. USB voltage powers the node transceiver as well as the support circuitry on the board. The master and Slave are connected by 4 lines (A, B, GND, and node detect signal).
Is it possible that a voltage transient on the communication lines somehow makes its way to the VCC?
If I am reading the circuit diagram from page 2 of the datasheet correctly, the diodes will clamp the voltage to 16 volts but a transient less than 16V will pass through?