HI
My customer would like to use the DAC904 with the following configuration :
"IOUT should be set to 20 mA.
For the generation of a single-ended signal we want to use a 50 ohm ADT2-1T (2:1 Transformer).
The output voltage is in one case be + / - 1V, otherwise 0 .. 2V.
I would IOUT and IOUT_inv (and not in a case, the center tap to GND, in the other case), each with 50 ohms to AGND wired
Then would by a 2:1 Transformer the output voltages achieved?"
regards,
kamal