Hi all.
There are the following questions about ADC12D1000.
1. At Time of Combination of One Master-ADC and One Slave-ADC,
For example, when one input signal is input into both a master and a slave,
Are the data in which the signal sample of the master-ADC was carried out,
and the data in which the signal sample of the slave-ADC was carried out outputted to the same timing with the almost same value?
2. Please let me know the input signal sampling of master and slave, and the details of data output timing.
3. Isn't there any graph to which the frequency of a CLK input and Jitter are related?.
Moreover, doesn't a problem have a CLK input a sign wave?
Best regards,
Hisa Kobayashi.