Hi,
i am using ADS4226 adc at 80MHz clock. when i capture the data i see there is clipping on I and Q plots. I do not see clipping at 10MHz clock input. When i send a ramp signal by setting 0x25 = 04 i do not see clipping. but when i feed 1.25MHz sine input at 150mvp-p with clock running at 80MHz i see clipping at the output of the ADC samples. what could be the issue? please suggest.
thanks