Hi,
The default analog input configuration is a transformer coupling through T1 and T2 for channel A, and T3 and T4 for channel B. There is an optional configuration for analog input is through an Operational-Amplifier (OPA), THS4509 on the ADS4226EVM.
I want to use the THS4509 for analog input, but the supply for THS4509 is dual supply.then, if it can be changed to single supply for THS4509 what should be done. In other words, which components should be installed except the component have illustrated in the Table 3 from SLAU333A document and the value of component should be changed.
Analog input from the AIN_CH-A J6, the range of signal is 1uv~10mV and the bandwidth is 125Mhz. The signal amplifies to 2-Vpp through THS4509, how to calculate the value for resistor relate to OPA-Driven Input circuit.
Schematic would be better for me. I really appreciate it.