Hi,
I am trying to use an ADS8343 ADC. I am going through the datasheet to figure out if this does what I need. I am looking for something that measure voltages between -2.5 and +2.5.
So far I think this chip will do it. But the way the COM and VREF pins are described is a little confusing. If I want my input ranges to be between -2.5 and +2.5, would I connect COM to 0V or VREF? The datasheet says COM should be connected to VREF, but then the graph afterwards shows VREF changing across 2.5V instead of 0V.
Any clarification would be appreciated.
Thanks,
Aditya