Hi,
is a ADS8363EVM kit compatible with MMB0 motherboard plate? I try to connect it to PC but I cannot see ADS8363EVM fomr ADCPRO. ADS1258EVM PDK works fine, for information. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
is a ADS8363EVM kit compatible with MMB0 motherboard plate? I try to connect it to PC but I cannot see ADS8363EVM fomr ADCPRO. ADS1258EVM PDK works fine, for information. Thank you.
Hi Tomaz!
Unfortunately it is not. Using the MMB0 is not an option because there is no way to synchronize the RD and CONVST signals needed to properly operate the ADS8363. The MMB0 was setup to interface with devices that have an SPI interface.
Hi Tom,
is there any other motherboard to evaluate ADS8363EVM plate? Or I need to implement EVM to my prototype circuit? It would be fine to use soma kind of motherboard to quick evaluate board. Thank you again.
Tomaz
Hi Tomaz,
Unfortunately no. I do have some sample code for a few TI processors though that you might find useful. What controller are you planning to use in this project?