This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3242 's road map?

Mastermind 6205 points

Replies: 2

Views: 356

 

Hello

My customer intends to use ADC for IF sigal sampling

RF(470-810MHz)-->Discrete Down Convert to IF(10.2MHz) ---Amp(THS4521) ---  ADC---Cyclone 4

*Requirements
-10bit or 12bit
-#2(2pcs)  or #4ch(1pcs)
-40MHz
-Serial LVDS interface
-SNR >60dB


Current candidate


1st  AD9219(ADI)  with 3.3V to 1.8V LDO
http://www.analog.com/static/imported-files/data_sheets/AD9219.pdf

2nd

ADS5240 but, 12bit is too rich  for their design.


So, 10bit /LVDS I/F  /40MHz is required

3rd   ADC10D40 but Parallel interface

4th   ADC3422   but there are no 10bit version
 

**

Q1  Do you have ADC324x 10bit version road map?


Q2  Woulr you please advise about  any counter plan to ADI's AD9219?
       Customer knows that they should have 1.8V LDO but its easy....

**

With My Best Regards

 

2 Replies

  • Hello,

    I am sorry, there were typo for part number on previour post

    ADC3422 ( LVDS/  50Mbps/quad ) is correct...but wish to have 10bit version

    Sorry for my typo.

     

     

  • In reply to KANJI SHIBATANI:

    Shibatani,

    you probably have found the best suitable options. Unfortunately there is no 10bit version of the ADC3422.

    Tommy

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.