Other Parts Discussed in Thread: ADS1298, ADCPRO
I am trying to set up the ADS1298 EVM and MMB0 motherboard with my PC (Windows 7).
I have installed ADCPro and ADS1298/8R EVM Evaluation Software. The MMB0 is recognized as an NI-VISA device in my Device Manager.
When I try to run the ADS1298 Eval SW, I get to the status message 'DSP not ready...Retrying' and then I get a firmware load error popup. The MMB0 is now an Unknown Device in Device Manager. I have to reset the MMB0 to correct that.
I tried going through the ADCPro Installation Manual (SLAU372A) but I get stuck at 4.2 USBStyx Driver Installation, that may be related to my problem.
Does the ADS1298 EVM have a plugin?
Is there a document that guides me through the setup of the MMB0 with the ADS1298 EVM? I have SBAU171C but that doesn't seem address my problem.
Thanks