Greetings:
I've attached a pdf schematic to reference with my questions.
My questions are:
1. The datasheet includes curves that indicate the maximum sink and source currents for this device. In the attached pdf, the DAC has a 1K resistor pullup on the analog output of the TLV5618A. This seems to violate the output sink current guidelines in the datasheet. Am I correct?
2. When the TLV5618A first powers up, what is the output voltage value, prior to the first time the DAC is written to over the serial link?
3. Is there a reason for needing the 1K pullup resistor that I am missing?
Thanks
Carl Reese
214-794-4897 cell;DAC_V_I.pdf