This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DAC5674 Sleep Pin Physical Connection

Intellectual 275 points

Replies: 1

Views: 287

Hello,

In the datasheet for the DAC5674, it states that SLEEP mode is activated by applying logic level 1 to the SLEEP pin (e.g. connecting SLEEP to AVdd).  In the electrical characteristics of the data sheet it has the following

 

However, on the eval board: DAC5674EVM, the schematics show the SLEEP pin connected to IOVdd which has a stated range of 1.65V to 3.6V in the datasheet.  Am I correct to assume that the SLEEP function will not work on the eval board if the IOVdd is 1.8V and not 3.3V.  Is this a mistake on the eval board?

 

Thanks,
Eric

  • Hi Eric,

    There is typo in the datasheet. The parameter should be 0.7 *IOVDD instead of AVDD.

    So to answer your question the SLEEP function will work with either 1.8V or 3.3V IOVDD.

    Regards

    Neeraj

    HSCC

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.