Hello,
Sorry if this should be a new thread, wasn't sure. I've made good progress using the board in my system using just the I channel. I am now feeding signals in the I and Q channel. In nonDES I and Q mode, 16K samples mode, it appears the board is sampling 8K from the I Channel and then sequentially sampling 8K from the Q channel. I would like to sample the two channels as close in time as possible. Is there a setting for an interlace sampling? I've verified my I and Q inputs separately using an o-scope to make sure the timings and triggers are all set up properly. I've also noticed the Q channel will not output anything when trying 32K samples mode, only the I channel shows the signal. Any ideas? Thank you for any help you can provide.
Justin