I am trying to communicate ADS131E8 from STM32F0 microcontroller. I also have DAC8564 on the same SPI bus and successfully write data to it. CPOL_Low, CPHA_2Edge. Looks it configured correctly.
SPI clock speed is about 185 KHz, which is slow enough.
DVDD connect to the same power line as microcontroller (3.3V), AVDD connects to own 3V regulator.
I run from internal clock (CLKSEL connected to DVDD), RESET and PWDN are not connected (I tried connect them to DVDD with no result)
I trying to read register 0x00 by sending following bytes to SPI: 0x11 0x20 0x01 0x00 0x00 0x00 0x00
The only response I got from ADS131 is DOUT pin becomes force low while is CS Low. DRDY keeps high independent on START pin state.
Also, what is the minimal external components requirements to run digital communication? I tried to communicate with other chip on other PCB, but do not want assemble it completely.
What could be a problem?