Hi,
I woule like to ask you some basic questions about ADS8422IB as below.
Would you please teach me?
1) No missing codes
About ADS8422IB, datasheet describes that the missing code is 16bits(MIN).
This means "there are not missing codes", I think.
But the DLE of ADS8422IB is specified -1(MIN), +/-0.7(TYP), 1.5(MAX) on the datasheet.
From this DLE value, I suppose the missing codes of ADS8422I is 15, not 16...
What is misunderstanding of my idea?
2) Resolution
About Resolution, as ILE is specified -2(MIN), +/-1(TYP), 2(MAX) on the datasheet, I think that the resolution of ADS8422IB is 14bit actulally.
(About ADS8422I, as the ILE is -6(MIN), +/-2(TYP), 6(MAX), the resolution is actually 10bit !?...)
Is my idea correct?
3) Input
What is "Fully Differential Input with Pseudo-Bipolar" ?
Thank you for your kindness.