What is the output of LM9833 and where to see it
is this IC pre programmed if not how to use this IC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the output of LM9833 and where to see it
is this IC pre programmed if not how to use this IC
Hello,
To answer your questions:
1. What is the output of LM9833 and where to see it?
Response: The 16 bit ADC data output(s) of the LM9833 are on pins D0 (LSB) -D15 (MSB).
2. Is this IC pre programmed if not how to use this IC?
Response: The LM9833 uses the USB digital interface for register read / write (pins SDA and SCL). The LM9833 registers have default power-on states, but there is significant periphery / external functionality required to make one of these "work". The device is meant to allow a system-on-a-chip solution for a scanner (including illumination control, motor control, etc.).
If you let me konw what you are planning to do, I might be able to offer more help.
Regards,
Hooman