Can the DAC882X series of converters be used in voltage reference mode as described herein: http://www.ti.com/lit/ug/tiduaf0/tiduaf0.pdf
thanks,chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chris,
In this case, you might still be able to use the TI Design that can use the DAC8820, but it still requires an output amplifier.
In order to pick the most appropriate device for your application I have a few more questions:
What output voltage range are you interested in generating?
What resolution is required?
What accuracy is required?
Howdy Chris,
I think what Eugenio's trying to point out is that with the DAC8822 device, you wouldn't need a negative supply, so there would be no need to connect it in the configuration that is displayed in the TI Design. For instance you can use one supply to connect to both Vref and VDD of the DAC8822 device when using it in the below configuration. Of course, you would need to pick a suitable operational amplifier that is capable of swinging from rail-to-rail.
Best Regards,
Matt
According to the previously suggested application note:
MDAC selection for this design is based on dc accuracy goals and the requirement of operating on a single-supply. Important parameters to consider for dc accuracy are gain error and linearity errors (INL and DNL). Since MDACs do not feature internal output amplifiers, they do not contribute offset error to the system output. In order to realize a design that operates on a single-supply the MDAC must provide external access to the IOUT2 node of the R-2R ladder.
and the DAC8822 does not, its IOUT2 is grounded. If i single-side the opamp then the feedback will try to drive it below 0V since everything is DC coupled.
Can i assume that the opamp could be biased midrail on + input and also be powered from the same single voltage source as the DAC and have everything swing between 0V and bias? see below?
Howdy Chris,
You are correct, I overlooked the second stage of the circuit (negative rail is required by OPA to produce negative output). A possible solution are the DAC8881 or DAC9881 device. These devices provide a positive unipolar output with positive supplies. IOVDD/DVDD/AVDD can connect together, allowing a single supply. The reference can also connect to this supply or connect to a REF device, as shown in the TIPD. Generally, the analog supplies are separated from the digital supplies to help reduce any digital noise from appearing on the analog output, so in this case you should expect digital noise to couple to the analog output. The only downside is that these devices exhibit larger glitch energy than other DACs in the precision portfolio (37nVs). The glitch can be reduced with either a simple low-pass, which will affect the bandwidth of the system, or with a one shot solution. Both solutions are explained in the URLs below:
e2e.ti.com/.../dac-essentials-glitch-be-gone
http://www.ti.com/tool/TIPD142
I've tried to find other MDAC devices similar to the DAC7811 (IOUT2) and with larger resolution, but haven't been able to filter any out. If this changes I will let you know and update this post.
Best Regards,
Matt