I have been trying tirelessly to change the text on the LCD screen in the ADS1118 MSP430 Boosterpack using the demo code. Once I finally downloaded and installed all of the extra packages I needed, the LCD screen would still not display what I wanted it to. It powers on, but the display remains blank. I tried loading the original demo code back onto the device, but nothing happened. Is there an updated version of the code that possibly does not use Grace? I am using a rev 1.5 MSP430G2553 launchpad. I noticed that the demo code was last modified in 2012.
The program has definitely been loaded onto the launchpad and nothing was changed in the code, but it still won't put the old program back on without flashing the program back to the device. I really just want to change what is being displayed on the LCD right now.
HELP!