Hello Everybody,
According to documentation, TIDA-00096 can give us 3-channel ECG with 160 samples per sec. Can we turn this module to 1-channel mode with 480 samples per sec.
Quote form doc (Wireless Heart-Rate Monitor Design Guide (Rev. A))
Bluetooth low-energy uses a 20-ms connection interval. Twenty user-data bytes (which is equal to 2- samples for each channel and 2-bytes running counter) are sent in GATT notifications. Data from ADS1293 device is ping-pong buffered and up to six notifications are sent every 14 ms based on an OSAL timer. The ADS1293 sample rate is set as 160 samples/sec (SPS) (see the ADS1293 data sheet, SNAS602,
Thank you in advance.