This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ADS4146 / Connecting EVM and FPGA

Guru 23440 points

Replies: 1

Views: 164

Hi,

My customer would like to connect ADS4146EVM and FPGA Board(DK-DEV-10M50-A).

I'm recognizing that ADS4146 EVM can connect with DK-DEV-10M50-A through HSMC (Altera) Header Adaptor Card.

www.ti.com/.../hsmc-adc-bridge

Is my understanding correct?

If there is things to be careful, please let me know.

Best Regards,

Kuramochi

  • Guru 63090 points

    Kuramochi,

    Attached is the Rev C schematic of the HSMC-ADC-Bridge card. I do not know what Altera board you are using but as long as the HSMC pins map to connector J1 on the bridge, the board should work just fine. There are a couple of signals that are connected to GND by the ADC board (pins 94, 96, 100, 102, 106, 108, 112 and 114). Just make sure there is not a problem with these being grounded on the Altera HSMC connector, which would be pins 66, 68, 60, 62, 54, 56, 48 and 50.

    Regards,

    Jim

    5824.SCH_HSMC_ADC_BRIDGE_REV_C.pdf

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.