Dear Technical Support Team
I have a question about ADS1211.
Is it better to issue reset sequence of "FIGURE 27. Resetting the ADS1210/11" every power up?
Datasheet shows " If the power supply ramp rate is greater than 50mV/ms, this circuit will be adequate to ensure that the device powers up correctly."
"If this requirement cannot be met or if the circuit has brown-out considerations, the timing diagram of Figure 27 can be used to reset the ADS1210/11. "
So I think that it is better to issue reset sequence if requirement is satisfied or not.
Best Regards,
y.i