This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Support for AMC1200



Hi Team,

 

One of our customer is comparing AMC1200B against ACPL-C79B-500E and need more clarifications on below parameters to compare spec2spec of parts. ACPL-C79B-500E is currently using in previous generation design and this is an opportunity for us to replace competition in high volume product and will also give entry to end customer AVL. Some the below mentioned parameters are given in the datasheet but customer need the values in same units as mentioned in competition datasheet.

 

Magnitude of Gain Change vs. Temperature in units of V/V/°C (different unit)

Magnitude of NL200 (non-linearity for 200mV) Change vs. Temperature in units of %/°C (not in datasheet)

Magnitude of Input Offset Change vs. Temperature in units of μV/°C (not in datasheet)

Input Bias Current (not in datasheet)

Magnitude of IIN+ Change vs. Temperature (not in datasheet)

Input to Output Propagation Delay 10%-10%, 50%-50%, 90%-90% for 200mV/us step input (comments:- given for 50 to 10%, 50-50% and 50-90%, as our parameters are mentioned for 500mV what will be for 200mV)

Output Voltage Range (not in datasheet)

Output Rise/Fall Time (10%-90%) for 200mV step input.(given for 500mV)

Signal to noise ratio (not in datasheet)

Lead solder temperature for 10sec. (not in datasheet)

 

Graphs of supply voltage (Vdd1 & Vdd2) vs gain and Gain vs temperature.

Thanks in advance for your help and support.

With Regards,

Shinu Mathew