Hello Team,
In regards to the ADS5562EVM I have a customer asking about the Break-out board that is used with this EVM.
I do not see that this board is included with the EVM. However in the user guide the following statement leads me to believe that it does come with this board.
http://www.ti.com/lit/ug/slwu061a/slwu061a.pdf
<Page 15 or section 2.2.4 Digital Outputs>
"Alternatively, the ADS61x9/55xx is supplied with a break-out board to easily connect the LVDS outputs to a logic analyzer pod. This LVDS break-out board also properly terminates the LVDS outputs once the breakout board is connected to J10."
Is this is a Typo? Or is this Break-out board supposed to be included with the EVM?
Any information is appreciated.
Have a great day!
Regards,
Ed Watts