Hi,
Which parameters should I use to caculate the ADC accuracy? The TUE , INL,DNL, Gain error or Offset error? Which formula can I use?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Which parameters should I use to caculate the ADC accuracy? The TUE , INL,DNL, Gain error or Offset error? Which formula can I use?
Hi user4411225
If your application is meant to oerform at room temperature then root sum square of typical value of INL, offset error and gain error will give you realistic ADC accuracy calculation at room temp
If application is supposed to work across temp range then take root sum square of max value of INL, offset error and gain error will give you realistic ADC accuracy calculation across temp
Can you please let me know more about end application
Thanks & Regards
Abhijeet
Hi Abhijeet,
Thanks for your quick replay. The ADS7253 is used to sample motor phase current in industry servo. I was told to caculate ADC accuracy in full work temp range. From what I understand, the ADC accuracy should be caculated by following formula:
ADC accuracy = TUE_max / (2^12)
TUE_max = sqrt (sq(Offset Error) + sq(Gain Error) + sq(DNL) + sq(INL)) with thermal drift;
The resolution of ADS7253 is 12bits, so is the denominator right?
Zhipan
Hi Zhipan
ADC specifications given in datasheet are for full scale range. You need not divide it by 2^12. You need to root sum square of gain error (%), INL (LSB) and oofset error.
If you know input range for your application then you can scale gain error accordingly to get more realistic number
Thanks & Regards
Abhijeet