I have the Waveshare Precision AD/DA board with the ads1256. I'm wanting to do a differential voltage and am using A0 and A1 as low voltage positive and negative inputs. The sample code for the ads1256 that comes with the board is in C and simply continuously scans all inputs and prints to my Raspberry Pi 3B's terminal. I'm new so forgive me, but I am under the impression I can gain a single value, the differential of the Vinp and Vinn values by using a "differential" mode. However I am not sure how to go about this. I will paste the code I have from the sample below. Thank you to anyone willing to help!
/* * ADS1256_test.c: * Very simple program to test the serial port. Expects * the port to be looped back to itself * */ /* define from bcm2835.h define from Board DVK511 3.3V | | 5V -> 3.3V | | 5V RPI_V2_GPIO_P1_03 | | 5V -> SDA | | 5V RPI_V2_GPIO_P1_05 | | GND -> SCL | | GND RPI_GPIO_P1_07 | | RPI_GPIO_P1_08 -> IO7 | | TX GND | | RPI_GPIO_P1_10 -> GND | | RX RPI_GPIO_P1_11 | | RPI_GPIO_P1_12 -> IO0 | | IO1 RPI_V2_GPIO_P1_13 | | GND -> IO2 | | GND RPI_GPIO_P1_15 | | RPI_GPIO_P1_16 -> IO3 | | IO4 VCC | | RPI_GPIO_P1_18 -> VCC | | IO5 RPI_GPIO_P1_19 | | GND -> MOSI | | GND RPI_GPIO_P1_21 | | RPI_GPIO_P1_22 -> MISO | | IO6 RPI_GPIO_P1_23 | | RPI_GPIO_P1_24 -> SCK | | CE0 GND | | RPI_GPIO_P1_26 -> GND | | CE1 ::if your raspberry Pi is version 1 or rev 1 or rev A RPI_V2_GPIO_P1_03->RPI_GPIO_P1_03 RPI_V2_GPIO_P1_05->RPI_GPIO_P1_05 RPI_V2_GPIO_P1_13->RPI_GPIO_P1_13 :: */ #include <bcm2835.h> #include <stdio.h> #include <unistd.h> #include <string.h> #include <math.h> #include <errno.h> //CS ----- SPICS //DIN ----- MOSI //DOUT ----- MISO //SCLK ----- SCLK //DRDY ----- ctl_IO data starting //RST ----- ctl_IO reset #define DRDY RPI_GPIO_P1_11 //P0 #define RST RPI_GPIO_P1_12 //P1 #define SPICS RPI_GPIO_P1_15 //P3 #define CS_1() bcm2835_gpio_write(SPICS,HIGH) #define CS_0() bcm2835_gpio_write(SPICS,LOW) #define DRDY_IS_LOW() ((bcm2835_gpio_lev(DRDY)==0)) #define RST_1() bcm2835_gpio_write(RST,HIGH); #define RST_0() bcm2835_gpio_write(RST,LOW); /* Unsigned integer types */ #define uint8_t unsigned char #define uint16_t unsigned short #define uint32_t unsigned long typedef enum {FALSE = 0, TRUE = !FALSE} bool; /* gain channelî */ typedef enum { ADS1256_GAIN_1 = (0), /* GAIN 1 */ ADS1256_GAIN_2 = (1), /*GAIN 2 */ ADS1256_GAIN_4 = (2), /*GAIN 4 */ ADS1256_GAIN_8 = (3), /*GAIN 8 */ ADS1256_GAIN_16 = (4), /* GAIN 16 */ ADS1256_GAIN_32 = (5), /*GAIN 32 */ ADS1256_GAIN_64 = (6), /*GAIN 64 */ }ADS1256_GAIN_E; /* Sampling speed choice*/ /* 11110000 = 30,000SPS (default) 11100000 = 15,000SPS 11010000 = 7,500SPS 11000000 = 3,750SPS 10110000 = 2,000SPS 10100001 = 1,000SPS 10010010 = 500SPS 10000010 = 100SPS 01110010 = 60SPS 01100011 = 50SPS 01010011 = 30SPS 01000011 = 25SPS 00110011 = 15SPS 00100011 = 10SPS 00010011 = 5SPS 00000011 = 2.5SPS */ typedef enum { ADS1256_30000SPS = 0, ADS1256_15000SPS, ADS1256_7500SPS, ADS1256_3750SPS, ADS1256_2000SPS, ADS1256_1000SPS, ADS1256_500SPS, ADS1256_100SPS, ADS1256_60SPS, ADS1256_50SPS, ADS1256_30SPS, ADS1256_25SPS, ADS1256_15SPS, ADS1256_10SPS, ADS1256_5SPS, ADS1256_2d5SPS, ADS1256_DRATE_MAX }ADS1256_DRATE_E; #define ADS1256_DRAE_COUNT = 15; typedef struct { ADS1256_GAIN_E Gain; /* GAIN */ ADS1256_DRATE_E DataRate; /* DATA output speed*/ int32_t AdcNow[8]; /* ADC Conversion value */ uint8_t Channel; /* The current channel*/ uint8_t ScanMode; /*Scanning mode, 0 Single-ended input 8 channel£¬ 1 Differential input 4 channel*/ }ADS1256_VAR_T; /*Register definition£º Table 23. Register Map --- ADS1256 datasheet Page 30*/ enum { /*Register address, followed by reset the default values */ REG_STATUS = 0, // x1H REG_MUX = 1, // 01H REG_ADCON = 2, // 20H REG_DRATE = 3, // F0H REG_IO = 4, // E0H REG_OFC0 = 5, // xxH REG_OFC1 = 6, // xxH REG_OFC2 = 7, // xxH REG_FSC0 = 8, // xxH REG_FSC1 = 9, // xxH REG_FSC2 = 10, // xxH }; /* Command definition£º TTable 24. Command Definitions --- ADS1256 datasheet Page 34 */ enum { CMD_WAKEUP = 0x00, // Completes SYNC and Exits Standby Mode 0000 0000 (00h) CMD_RDATA = 0x01, // Read Data 0000 0001 (01h) CMD_RDATAC = 0x03, // Read Data Continuously 0000 0011 (03h) CMD_SDATAC = 0x0F, // Stop Read Data Continuously 0000 1111 (0Fh) CMD_RREG = 0x10, // Read from REG rrr 0001 rrrr (1xh) CMD_WREG = 0x50, // Write to REG rrr 0101 rrrr (5xh) CMD_SELFCAL = 0xF0, // Offset and Gain Self-Calibration 1111 0000 (F0h) CMD_SELFOCAL= 0xF1, // Offset Self-Calibration 1111 0001 (F1h) CMD_SELFGCAL= 0xF2, // Gain Self-Calibration 1111 0010 (F2h) CMD_SYSOCAL = 0xF3, // System Offset Calibration 1111 0011 (F3h) CMD_SYSGCAL = 0xF4, // System Gain Calibration 1111 0100 (F4h) CMD_SYNC = 0xFC, // Synchronize the A/D Conversion 1111 1100 (FCh) CMD_STANDBY = 0xFD, // Begin Standby Mode 1111 1101 (FDh) CMD_RESET = 0xFE, // Reset to Power-Up Values 1111 1110 (FEh) }; ADS1256_VAR_T g_tADS1256; static const uint8_t s_tabDataRate[ADS1256_DRATE_MAX] = { 0xF0, /*reset the default values */ 0xE0, 0xD0, 0xC0, 0xB0, 0xA1, 0x92, 0x82, 0x72, 0x63, 0x53, 0x43, 0x33, 0x20, 0x13, 0x03 }; void bsp_DelayUS(uint64_t micros); void ADS1256_StartScan(uint8_t _ucScanMode); static void ADS1256_Send8Bit(uint8_t _data); void ADS1256_CfgADC(ADS1256_GAIN_E _gain, ADS1256_DRATE_E _drate); static void ADS1256_DelayDATA(void); static uint8_t ADS1256_Recive8Bit(void); static void ADS1256_WriteReg(uint8_t _RegID, uint8_t _RegValue); static uint8_t ADS1256_ReadReg(uint8_t _RegID); static void ADS1256_WriteCmd(uint8_t _cmd); uint8_t ADS1256_ReadChipID(void); static void ADS1256_SetChannal(uint8_t _ch); static void ADS1256_SetDiffChannal(uint8_t _ch); static void ADS1256_WaitDRDY(void); static int32_t ADS1256_ReadData(void); int32_t ADS1256_GetAdc(uint8_t _ch); void ADS1256_ISR(void); uint8_t ADS1256_Scan(void); void bsp_DelayUS(uint64_t micros) { bcm2835_delayMicroseconds (micros); } /* ********************************************************************************************************* * name: bsp_InitADS1256 * function: Configuration of the STM32 GPIO and SPI interface£¬The connection ADS1256 * parameter: NULL * The return value: NULL ********************************************************************************************************* */ void bsp_InitADS1256(void) { #ifdef SOFT_SPI CS_1(); SCK_0(); DI_0(); #endif //ADS1256_CfgADC(ADS1256_GAIN_1, ADS1256_1000SPS); /* ÅäÖÃADC²ÎÊý£º ÔöÒæ1:1, Êý¾ÝÊä³öËÙÂÊ 1KHz */ } /* ********************************************************************************************************* * name: ADS1256_StartScan * function: Configuration DRDY PIN for external interrupt is triggered * parameter: _ucDiffMode : 0 Single-ended input 8 channel£¬ 1 Differential input 4 channe * The return value: NULL ********************************************************************************************************* */ void ADS1256_StartScan(uint8_t _ucScanMode) { g_tADS1256.ScanMode = _ucScanMode; /* ¿ªÊ¼É¨ÃèÇ°, ÇåÁã½á¹û»º³åÇø */ { uint8_t i; g_tADS1256.Channel = 0; for (i = 0; i < 8; i++) { g_tADS1256.AdcNow[i] = 0; } } } /* ********************************************************************************************************* * name: ADS1256_Send8Bit * function: SPI bus to send 8 bit data * parameter: _data: data * The return value: NULL ********************************************************************************************************* */ static void ADS1256_Send8Bit(uint8_t _data) { bsp_DelayUS(2); bcm2835_spi_transfer(_data); } /* ********************************************************************************************************* * name: ADS1256_CfgADC * function: The configuration parameters of ADC, gain and data rate * parameter: _gain:gain 1-64 * _drate: data rate * The return value: NULL ********************************************************************************************************* */ void ADS1256_CfgADC(ADS1256_GAIN_E _gain, ADS1256_DRATE_E _drate) { g_tADS1256.Gain = _gain; g_tADS1256.DataRate = _drate; ADS1256_WaitDRDY(); { uint8_t buf[4]; /* Storage ads1256 register configuration parameters */ /*Status register define Bits 7-4 ID3, ID2, ID1, ID0 Factory Programmed Identification Bits (Read Only) Bit 3 ORDER: Data Output Bit Order 0 = Most Significant Bit First (default) 1 = Least Significant Bit First Input data is always shifted in most significant byte and bit first. Output data is always shifted out most significant byte first. The ORDER bit only controls the bit order of the output data within the byte. Bit 2 ACAL : Auto-Calibration 0 = Auto-Calibration Disabled (default) 1 = Auto-Calibration Enabled When Auto-Calibration is enabled, self-calibration begins at the completion of the WREG command that changes the PGA (bits 0-2 of ADCON register), DR (bits 7-0 in the DRATE register) or BUFEN (bit 1 in the STATUS register) values. Bit 1 BUFEN: Analog Input Buffer Enable 0 = Buffer Disabled (default) 1 = Buffer Enabled Bit 0 DRDY : Data Ready (Read Only) This bit duplicates the state of the DRDY pin. ACAL=1 enable calibration */ //buf[0] = (0 << 3) | (1 << 2) | (1 << 1);//enable the internal buffer buf[0] = (0 << 3) | (1 << 2) | (0 << 1); // The internal buffer is prohibited //ADS1256_WriteReg(REG_STATUS, (0 << 3) | (1 << 2) | (1 << 1)); buf[1] = 0x08; /* ADCON: A/D Control Register (Address 02h) Bit 7 Reserved, always 0 (Read Only) Bits 6-5 CLK1, CLK0 : D0/CLKOUT Clock Out Rate Setting 00 = Clock Out OFF 01 = Clock Out Frequency = fCLKIN (default) 10 = Clock Out Frequency = fCLKIN/2 11 = Clock Out Frequency = fCLKIN/4 When not using CLKOUT, it is recommended that it be turned off. These bits can only be reset using the RESET pin. Bits 4-3 SDCS1, SCDS0: Sensor Detect Current Sources 00 = Sensor Detect OFF (default) 01 = Sensor Detect Current = 0.5 ¦Ì A 10 = Sensor Detect Current = 2 ¦Ì A 11 = Sensor Detect Current = 10¦Ì A The Sensor Detect Current Sources can be activated to verify the integrity of an external sensor supplying a signal to the ADS1255/6. A shorted sensor produces a very small signal while an open-circuit sensor produces a very large signal. Bits 2-0 PGA2, PGA1, PGA0: Programmable Gain Amplifier Setting 000 = 1 (default) 001 = 2 010 = 4 011 = 8 100 = 16 101 = 32 110 = 64 111 = 64 */ buf[2] = (0 << 5) | (0 << 3) | (_gain << 0); //ADS1256_WriteReg(REG_ADCON, (0 << 5) | (0 << 2) | (GAIN_1 << 1)); /*choose 1: gain 1 ;input 5V/ buf[3] = s_tabDataRate[_drate]; // DRATE_10SPS; CS_0(); /* SPIƬѡ = 0 */ ADS1256_Send8Bit(CMD_WREG | 0); /* Write command register, send the register address */ ADS1256_Send8Bit(0x03); /* Register number 4,Initialize the number -1*/ ADS1256_Send8Bit(buf[0]); /* Set the status register */ ADS1256_Send8Bit(buf[1]); /* Set the input channel parameters */ ADS1256_Send8Bit(buf[2]); /* Set the ADCON control register,gain */ ADS1256_Send8Bit(buf[3]); /* Set the output rate */ CS_1(); /* SPI cs = 1 */ } bsp_DelayUS(50); } /* ********************************************************************************************************* * name: ADS1256_DelayDATA * function: delay * parameter: NULL * The return value: NULL ********************************************************************************************************* */ static void ADS1256_DelayDATA(void) { /* Delay from last SCLK edge for DIN to first SCLK rising edge for DOUT: RDATA, RDATAC,RREG Commands min 50 CLK = 50 * 0.13uS = 6.5uS */ bsp_DelayUS(10); /* The minimum time delay 6.5us */ } /* ********************************************************************************************************* * name: ADS1256_Recive8Bit * function: SPI bus receive function * parameter: NULL * The return value: NULL ********************************************************************************************************* */ static uint8_t ADS1256_Recive8Bit(void) { uint8_t read = 0; read = bcm2835_spi_transfer(0xff); return read; } /* ********************************************************************************************************* * name: ADS1256_WriteReg * function: Write the corresponding register * parameter: _RegID: register ID * _RegValue: register Value * The return value: NULL ********************************************************************************************************* */ static void ADS1256_WriteReg(uint8_t _RegID, uint8_t _RegValue) { CS_0(); /* SPI cs = 0 */ ADS1256_Send8Bit(CMD_WREG | _RegID); /*Write command register */ ADS1256_Send8Bit(0x00); /*Write the register number */ ADS1256_Send8Bit(_RegValue); /*send register value */ CS_1(); /* SPI cs = 1 */ } /* ********************************************************************************************************* * name: ADS1256_ReadReg * function: Read the corresponding register * parameter: _RegID: register ID * The return value: read register value ********************************************************************************************************* */ static uint8_t ADS1256_ReadReg(uint8_t _RegID) { uint8_t read; CS_0(); /* SPI cs = 0 */ ADS1256_Send8Bit(CMD_RREG | _RegID); /* Write command register */ ADS1256_Send8Bit(0x00); /* Write the register number */ ADS1256_DelayDATA(); /*delay time */ read = ADS1256_Recive8Bit(); /* Read the register values */ CS_1(); /* SPI cs = 1 */ return read; } /* ********************************************************************************************************* * name: ADS1256_WriteCmd * function: Sending a single byte order * parameter: _cmd : command * The return value: NULL ********************************************************************************************************* */ static void ADS1256_WriteCmd(uint8_t _cmd) { CS_0(); /* SPI cs = 0 */ ADS1256_Send8Bit(_cmd); CS_1(); /* SPI cs = 1 */ } /* ********************************************************************************************************* * name: ADS1256_ReadChipID * function: Read the chip ID * parameter: _cmd : NULL * The return value: four high status register ********************************************************************************************************* */ uint8_t ADS1256_ReadChipID(void) { uint8_t id; ADS1256_WaitDRDY(); id = ADS1256_ReadReg(REG_STATUS); return (id >> 4); } /* ********************************************************************************************************* * name: ADS1256_SetChannal * function: Configuration channel number * parameter: _ch: channel number 0--7 * The return value: NULL ********************************************************************************************************* */ static void ADS1256_SetChannal(uint8_t _ch) { /* Bits 7-4 PSEL3, PSEL2, PSEL1, PSEL0: Positive Input Channel (AINP) Select 0000 = AIN0 (default) 0001 = AIN1 0010 = AIN2 (ADS1256 only) 0011 = AIN3 (ADS1256 only) 0100 = AIN4 (ADS1256 only) 0101 = AIN5 (ADS1256 only) 0110 = AIN6 (ADS1256 only) 0111 = AIN7 (ADS1256 only) 1xxx = AINCOM (when PSEL3 = 1, PSEL2, PSEL1, PSEL0 are ¡°don¡¯t care¡±) NOTE: When using an ADS1255 make sure to only select the available inputs. Bits 3-0 NSEL3, NSEL2, NSEL1, NSEL0: Negative Input Channel (AINN)Select 0000 = AIN0 0001 = AIN1 (default) 0010 = AIN2 (ADS1256 only) 0011 = AIN3 (ADS1256 only) 0100 = AIN4 (ADS1256 only) 0101 = AIN5 (ADS1256 only) 0110 = AIN6 (ADS1256 only) 0111 = AIN7 (ADS1256 only) 1xxx = AINCOM (when NSEL3 = 1, NSEL2, NSEL1, NSEL0 are ¡°don¡¯t care¡±) */ if (_ch > 7) { return; } ADS1256_WriteReg(REG_MUX, (_ch << 4) | (1 << 3)); /* Bit3 = 1, AINN connection AINCOM */ } /* ********************************************************************************************************* * name: ADS1256_SetDiffChannal * function: The configuration difference channel * parameter: _ch: channel number 0--3 * The return value: four high status register ********************************************************************************************************* */ static void ADS1256_SetDiffChannal(uint8_t _ch) { /* Bits 7-4 PSEL3, PSEL2, PSEL1, PSEL0: Positive Input Channel (AINP) Select 0000 = AIN0 (default) 0001 = AIN1 0010 = AIN2 (ADS1256 only) 0011 = AIN3 (ADS1256 only) 0100 = AIN4 (ADS1256 only) 0101 = AIN5 (ADS1256 only) 0110 = AIN6 (ADS1256 only) 0111 = AIN7 (ADS1256 only) 1xxx = AINCOM (when PSEL3 = 1, PSEL2, PSEL1, PSEL0 are ¡°don¡¯t care¡±) NOTE: When using an ADS1255 make sure to only select the available inputs. Bits 3-0 NSEL3, NSEL2, NSEL1, NSEL0: Negative Input Channel (AINN)Select 0000 = AIN0 0001 = AIN1 (default) 0010 = AIN2 (ADS1256 only) 0011 = AIN3 (ADS1256 only) 0100 = AIN4 (ADS1256 only) 0101 = AIN5 (ADS1256 only) 0110 = AIN6 (ADS1256 only) 0111 = AIN7 (ADS1256 only) 1xxx = AINCOM (when NSEL3 = 1, NSEL2, NSEL1, NSEL0 are ¡°don¡¯t care¡±) */ if (_ch == 0) { ADS1256_WriteReg(REG_MUX, (0 << 4) | 1); /* DiffChannal AIN0£¬ AIN1 */ } else if (_ch == 1) { ADS1256_WriteReg(REG_MUX, (2 << 4) | 3); /*DiffChannal AIN2£¬ AIN3 */ } else if (_ch == 2) { ADS1256_WriteReg(REG_MUX, (4 << 4) | 5); /*DiffChannal AIN4£¬ AIN5 */ } else if (_ch == 3) { ADS1256_WriteReg(REG_MUX, (6 << 4) | 7); /*DiffChannal AIN6£¬ AIN7 */ } } /* ********************************************************************************************************* * name: ADS1256_WaitDRDY * function: delay time wait for automatic calibration * parameter: NULL * The return value: NULL ********************************************************************************************************* */ static void ADS1256_WaitDRDY(void) { uint32_t i; for (i = 0; i < 400000; i++) { if (DRDY_IS_LOW()) { break; } } if (i >= 400000) { printf("ADS1256_WaitDRDY() Time Out ...\r\n"); } } /* ********************************************************************************************************* * name: ADS1256_ReadData * function: read ADC value * parameter: NULL * The return value: NULL ********************************************************************************************************* */ static int32_t ADS1256_ReadData(void) { uint32_t read = 0; static uint8_t buf[3]; CS_0(); /* SPI cs = 0 */ ADS1256_Send8Bit(CMD_RDATA); /* read ADC command */ ADS1256_DelayDATA(); /*delay time */ /*Read the sample results 24bit*/ buf[0] = ADS1256_Recive8Bit(); buf[1] = ADS1256_Recive8Bit(); buf[2] = ADS1256_Recive8Bit(); read = ((uint32_t)buf[0] << 16) & 0x00FF0000; read |= ((uint32_t)buf[1] << 8); /* Pay attention to It is wrong read |= (buf[1] << 8) */ read |= buf[2]; CS_1(); /* SPIƬѡ = 1 */ /* Extend a signed number*/ if (read & 0x800000) { read |= 0xFF000000; } return (int32_t)read; } /* ********************************************************************************************************* * name: ADS1256_GetAdc * function: read ADC value * parameter: channel number 0--7 * The return value: ADC vaule (signed number) ********************************************************************************************************* */ int32_t ADS1256_GetAdc(uint8_t _ch) { int32_t iTemp; if (_ch > 7) { return 0; } iTemp = g_tADS1256.AdcNow[_ch]; return iTemp; } /* ********************************************************************************************************* * name: ADS1256_ISR * function: Collection procedures * parameter: NULL * The return value: NULL ********************************************************************************************************* */ void ADS1256_ISR(void) { if (g_tADS1256.ScanMode == 0) /* 0 Single-ended input 8 channel£¬ 1 Differential input 4 channe */ { ADS1256_SetChannal(g_tADS1256.Channel); /*Switch channel mode */ bsp_DelayUS(5); ADS1256_WriteCmd(CMD_SYNC); bsp_DelayUS(5); ADS1256_WriteCmd(CMD_WAKEUP); bsp_DelayUS(25); if (g_tADS1256.Channel == 0) { g_tADS1256.AdcNow[7] = ADS1256_ReadData(); } else { g_tADS1256.AdcNow[g_tADS1256.Channel-1] = ADS1256_ReadData(); } if (++g_tADS1256.Channel >= 8) { g_tADS1256.Channel = 0; } } else /*DiffChannal*/ { ADS1256_SetDiffChannal(g_tADS1256.Channel); /* change DiffChannal */ bsp_DelayUS(5); ADS1256_WriteCmd(CMD_SYNC); bsp_DelayUS(5); ADS1256_WriteCmd(CMD_WAKEUP); bsp_DelayUS(25); if (g_tADS1256.Channel == 0) { g_tADS1256.AdcNow[3] = ADS1256_ReadData(); } else { g_tADS1256.AdcNow[g_tADS1256.Channel-1] = ADS1256_ReadData(); } if (++g_tADS1256.Channel >= 4) { g_tADS1256.Channel = 0; } } } /* ********************************************************************************************************* * name: ADS1256_Scan * function: * parameter:NULL * The return value: 1 ********************************************************************************************************* */ uint8_t ADS1256_Scan(void) { if (DRDY_IS_LOW()) { ADS1256_ISR(); return 1; } return 0; } /* ********************************************************************************************************* * name: Write_DAC8552 * function: DAC send data * parameter: channel : output channel number * data : output DAC value * The return value: NULL ********************************************************************************************************* */ void Write_DAC8552(uint8_t channel, uint16_t Data) { uint8_t i; CS_1() ; CS_0() ; bcm2835_spi_transfer(channel); bcm2835_spi_transfer((Data>>8)); bcm2835_spi_transfer((Data&0xff)); CS_1() ; } /* ********************************************************************************************************* * name: Voltage_Convert * function: Voltage value conversion function * parameter: Vref : The reference voltage 3.3V or 5V * voltage : output DAC value * The return value: NULL ********************************************************************************************************* */ uint16_t Voltage_Convert(float Vref, float voltage) { uint16_t _D_; _D_ = (uint16_t)(65536 * voltage / Vref); return _D_; } /* ********************************************************************************************************* * name: main * function: * parameter: NULL * The return value: NULL ********************************************************************************************************* */ int main() { uint8_t id; int32_t adc[8]; int32_t volt[8]; uint8_t i; uint8_t ch_num; int32_t iTemp; uint8_t buf[3]; if (!bcm2835_init()) return 1; bcm2835_spi_begin(); bcm2835_spi_setBitOrder(BCM2835_SPI_BIT_ORDER_LSBFIRST ); // The default bcm2835_spi_setDataMode(BCM2835_SPI_MODE1); // The default bcm2835_spi_setClockDivider(BCM2835_SPI_CLOCK_DIVIDER_1024); // The default bcm2835_gpio_fsel(SPICS, BCM2835_GPIO_FSEL_OUTP);// bcm2835_gpio_write(SPICS, HIGH); bcm2835_gpio_fsel(DRDY, BCM2835_GPIO_FSEL_INPT); bcm2835_gpio_set_pud(DRDY, BCM2835_GPIO_PUD_UP); //ADS1256_WriteReg(REG_MUX,0x01); //ADS1256_WriteReg(REG_ADCON,0x20); // ADS1256_CfgADC(ADS1256_GAIN_1, ADS1256_15SPS); id = ADS1256_ReadChipID(); printf("\r\n"); printf("ID=\r\n"); if (id != 3) { printf("Error, ASD1256 Chip ID = 0x%d\r\n", (int)id); } else { printf("Ok, ASD1256 Chip ID = 0x%d\r\n", (int)id); } ADS1256_CfgADC(ADS1256_GAIN_1, ADS1256_15SPS); ADS1256_StartScan(0); ch_num = 8; //if (ADS1256_Scan() == 0) //{ //continue; //} while(1) { while((ADS1256_Scan() == 0)); for (i = 0; i < ch_num; i++) { adc[i] = ADS1256_GetAdc(i); volt[i] = (adc[i] * 100) / 167; } for (i = 0; i < ch_num; i++) { buf[0] = ((uint32_t)adc[i] >> 16) & 0xFF; buf[1] = ((uint32_t)adc[i] >> 8) & 0xFF; buf[2] = ((uint32_t)adc[i] >> 0) & 0xFF; printf("%d=%02X%02X%02X, %8ld", (int)i, (int)buf[0], (int)buf[1], (int)buf[2], (long)adc[i]); iTemp = volt[i]; /* uV */ if (iTemp < 0) { iTemp = -iTemp; printf(" (-%ld.%03ld %03ld V) \r\n", iTemp /1000000, (iTemp%1000000)/1000, iTemp%1000); } else { printf(" ( %ld.%03ld %03ld V) \r\n", iTemp /1000000, (iTemp%1000000)/1000, iTemp%1000); } } printf("\33[%dA", (int)ch_num); bsp_DelayUS(100000); } bcm2835_spi_end(); bcm2835_close(); return 0; }