Part Number: TSW1400EVM
Other Parts Discussed in Thread: ADS54RF63, ADS54RF63EVM
I have remove R61 R62 R63 R64
and install R55 R57 R58 R59 R60 R129
and the R55 is 1k.
but the jtag chain doesn't work;
can you give me some advice
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSW1400EVM
Other Parts Discussed in Thread: ADS54RF63, ADS54RF63EVM
I have remove R61 R62 R63 R64
and install R55 R57 R58 R59 R60 R129
and the R55 is 1k.
but the jtag chain doesn't work;
can you give me some advice
I just reverified this on a revD EVM - works as expected.
R55=1k
R57/58/59/60/129 = 0
R61/62/63/64 = remove
I started up Quartus programmer, ensured the the USB Blaster was connected properly, did a scan and it found the Stratix IV FPGA.
If this works then you can use the JTAG as you normally would with Quartus. If not check your soldering.
Ken
HI
KEN
It just a register is not welded firmly.
the change can work succesful,
Can i still use the HSDC?
i will very happy if you can give me a example about tsw1400.
Another qusetion : How to get a reliable clock input for ads54rf63.
how about the clk from tsw1400'board?
THANKS
THANKS
Hi,
Yes you can still use the register and SPI access ports to the TSW1400 from HSDC Pro. Typically you would load the firmware first using JTAG then start HSDC Pro. It will attempt to communicate with the firmware to confirm if it already has a loaded firmware.
However if you modify the firmware, HSDC Pro may or may not work with the new firmware. There is no guarantee, HSDC Pro is only guaranteed to work with our official released/tested firmware.
Ken
Hi,
I do not have any files to use with Quartus and JTAG. You will need to generate a sof or pof firmware file to load via Quartus.
Ken