Hi Team,
Please advise me on questions bellow.
The figure 98 on the ADS6142 datasheet illustrates application circuit.
Q1. Two 200 ohm resisters are used as the VCM bias circuit.
Can they be substitute with two 220 ohm resisters or two 180 ohm resisters?
If resisters other than 200 ohm are used what performance degradations are expected?
Q2. Two 5 ohm resisters are used in series to the differential analog input pins.
Can they be substitute with two 4.8 ohm resisters or two 5.6 ohm resisters?
If resisters other than 5 ohm are used what performance degradations are expected?
Mita