Hi,
I'm making a 3 phase buck converter and I need 3 phase current measurements (1 for each phase) and 1 voltage measurement (output voltage).
In my current schematic I have it set up so that the current measurement is between the switch and the inductor. I had problems with long delta sigma lines to the uP. It got me thinking that large (to 900V ) voltage swings at the switch node are not going to be good for good measurements.
1) Placing the 3 current measurements between the inductors and output capacitor would be batter because of the stabler CMV, right?
2,3) Could I then use 1 ISO power supply to supply all 4 insulated measurements? The 3 currents and the voltage sensing are going to have the same "ISO GND" that will be the V+ off the capacitor. For the voltage measurement I will then have to use the first resistor in the resistor divider ladder. Now I have it sensing form the middle of the resistor divider ladder, this was, in past experiences better. Would this be a problem?
I know if I use 1 power supply I will have to make good decoupling, maybe some ferite beds for each ADC to keep the power supply noise down.
Best regards,
Marko