Other Parts Discussed in Thread: ADS1298ECGFE-PDK, TMS320VC5509A, ADS1298
I bought the ADS1298ECGFE-PDK and I try to make some test measurements.
I've downloaded the newest software 0.7.1 and follow the install steps from the file "sbau171.pdf" p.11-13.
The installation seems fine but than Windows cannot install the driver properly. I mean in the user guide at p.11-13
there is no information about installing drivers. It seems that you just press 3x "Next" and then everything should work.
But it doesn't.
When I try to install the driver manually from "..\ADS1298ECG-FE\driver" it also doesn't work.
The following warning appears:
There was a problem installing this hardware:
TMS320VC5509A (NI-VISA)
An error occurred during the installation of the device
The system cannot find the file specified
Then after repeating this step several time sometimes this warning appears:
There was a problem installing this hardware:
USBStyx
An error occurred during the installation of the device
The system cannot find the file specified
I also try to install the driver manually from "..\ADS1298ECG-FE\libmmb0\Styx\driver-win32" it also
doesn't work.
I looked up in the Device Manager and the device is not installed:
When I start the software sometimes it works to get the firmware version.
But as far as I press for example the "Acquire" or "Continous" Button this error appears:
And nothing works anymore
The tests were all done with a WinXP SP2 system.
What are the problems with the drivers?
I hope anybody can help!!
best regards