This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC104S085: DAC104S085 WITH r daisy-chain

Guru 13485 points
Part Number: DAC104S085
Other Parts Discussed in Thread: DAC60004, DAC60504, DAC70504, DAC7716

Looking a replacement to LTC2634, a quad 12bit with FSO  above 2.04V (preferred closed to 5V) ,similr to DAC104S085, but with DAISY CHAIN OPERATION!!!!

  • Hi Eli,

    Thank you for your query. Please find the options:

    1. If you don't need an internal reference, you can go for DAC60004
    2. If you need an internal reference, you can look into DAC70504. It's a 14-bit DAC but the 12-bit version (DAC60504) is going to be released shortly. This should cater all your requirements
    3. You can also look into DAC7716 in case you need higher voltage

    Hope I have answered your question.

    Regards,
    Uttam Sahu
    Applications Engineer, Precision DACs