Hi all
Would you mind if we ask ADS7253?
<Question1>
On the datasheet P9. there is the description about Reference output dc current (I_REFOUT)=2mA(typ).
It means that if I_REFOUT is within 2mA, V_REFOUT can keep 2.500V.
Is our recognition correct?
And why does this I_REFOUT=2mA mean typical value?(or Max value?)
<Question2>
Does (I_REFOUT)=2mA(typ) mean source and sink?(Or only source?)
<Question3>
Does the value (I_REFOUT)=2mA(typ) contain REFIO_A and REFIO_B?
So, is total 2mA(typ)?
Or is each value 2mA(typ)?
<Question4>
On the datasheet P9. there is the description about Internal reference output impedance RO=1Ω(Typ).
Could you let us know max value?
Kind regards,
Hirotaka Matsumoto