This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ADS5400EVM: to ADC FMC Adapter to Xilinx ZC706 board question

Prodigy 30 points

Replies: 1

Views: 475

Part Number: ADS5400EVM

Greetings

I am having trouble routing the CLKOUT signal from the ADC board to the ZC706 board and using it as a clock.

The pins I am interested are shown here on the evm,

  

Then routed to the FMC ADC adapter board

Which routes to a non-clock pin on the ZC706

V23   IO_L24P_T3_13            3                  13    NA            NA                  HR        NA
W24   IO_L24N_T3_13            3                  13    NA            NA                  HR        NA

However the DA5(on the EVM) does route to a clock capable pin,

Is my understanding of all this correct?

I my intention was to drive my FPGA with the the output clock from the ADS board.

Thank you!

-Emil C

  • Guru 61680 points

    Emil,

    You are correct. The adapter board was designed and released several years before the ZC706 came out. Due to this, there may be issues like this.

    Regards,

    Jim 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.