Hey TI Community,
I'm new in this whole DAC world, so I hope I'm right here with my questions.
We need a 16bit 4 channel DAC with differential outputs for controlling electric engines. Because of a short time plan we can't design our own board, so the best solution will be a evaluation module. The requirements are not very high, the sample rate is 500kHz maximum. We want to connect the EVM with a Opal Kelly XEM7350 board, because it has a FMC-HPC connector and we can easily communicate with it via sofware.
Make this set up sense or is there a DAC-EVM which is better for this task? According to the pictures of this board the analog outputs are not differential. Is it possible to add the analog outputs for a differential signal or are they grounded?
Thank you for your support, best regards
Michael