Comrades, We purchased two of the DAC37J82EVM boards and a TSW14J56EVM. Using DAC3XJ8X GUI v1.1 & HS Data Convertor Pro v4.80. When running the Quick Setup the first board programmed and ran the demo once, but then wouldn't work again. The 2nd board did the same? Any ideas? Do you definitely need USB 3.0 for the TSW? I believe the PC I'm using on only has USB 2.0. The LMK and the TSW seems to program fine, but the DAC tool reports the PLLs unlocked, though I can see they are lock per the LEDs. Any ideas would be greatly appreciated.