Hi,
This is the part that I am not sure:
"The input common-mode is set internally using a 5-kΩ resistor from each input pin to VCM so the input signal
can be ac-coupled to the pins."
Does this mean I have to put an external resistor in series from VCM to each leg?
Does it mean I don't have to worry about external resistor because they are all internally connected?
I know it is a basic question but I really need clarification.
Thanks.