Part Number: ADC12D1800RFRB
HI,
I trying to capture data from ADC via ML-605. When i using Pin trigger in the TI GHz ADC the data that I captured is not capture the same time.How can I do it?. Or can I use the time stamp or not?
Thank you,
P.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC12D1800RFRB
HI,
I trying to capture data from ADC via ML-605. When i using Pin trigger in the TI GHz ADC the data that I captured is not capture the same time.How can I do it?. Or can I use the time stamp or not?
Thank you,
P.
Hi Pachara
I'm not very familiar with that older ML-605 capture firmware, but my guess is that the trigger input is re-sampled by a clock running at some lower frequency than the ADC sample clock. If the trigger source is not synchronous to this internal re-sampling clock there will be variable latency from the trigger rising edge to the apparent start of data in the captured record, for the ADC sampling at the full clock rate.
Best regards,
Jim B